AXIS#.LOAD.INERTIA
Description
AXIS#.LOAD.INERTIA sets the load inertia.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
kgcm² for rotary motors |
|
Range |
1 to 1,000,000 kgcm² or kg |
|
Default Value |
0 kgcm² or kg |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.LOAD.INERTIA | 0x5014 | 0x1 | UDINT | 1000:1 | - | RW | False |
| AXIS2.LOAD.INERTIA | 0x5114 | 0x1 | UDINT | 1000:1 | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|